FB#.ENCLINES
Description
Used to configure the number of lines per revolution for rotary encoders. This keyword is only valid for Incremental and Sin/Cos encoders and will be ignored for any other encoders and linear motors. For linear motors, see FB#.LINEPITCH.
Examples
Context
See Feedback.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Read/Write |
|
Units |
Lines/Rev |
|
Range |
0 to 4,294,967,288 |
|
Default Value |
1024 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | FB1.ENCLINES | 0x3500 | 0x2 | UDINT | - | - | RW | False |
| FB2.ENCLINES | 0x3501 | 0x2 | UDINT | - | - | RW | False | |
| FB3.ENCLINES | 0x3502 | 0x2 | UDINT | - | - | RW | False | |
| FB4.ENCLINES | 0x3503 | 0x2 | UDINT | - | - | RW | False | |
| FB5.ENCLINES | 0x3504 | 0x2 | UDINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|